(1)| 6/28/2011 3:35 PM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Please read the attachment about SFC58,SFC59 to undrestand their operation and requirement much better.The LADDR is module base address which can be found in H.W config editor. More information about SFCs here: System Software for S7-300/400 System and Standard Functions Volume 1 and Volume 2 Regards AttachmentSFC58_59.pdf (1797 Downloads) |
| 6/29/2011 10:18 AM | |
|
Posts: 133 Rating:
|
Sorry but i dont understand what is parameter LADDR,in HW configuration i have 1 and 10 as profibus address for the slaves |
| 6/29/2011 10:55 AM | |
|
Posts: 133 Rating:
|
ok understood, thanks |
This contribution was helpful to
|
|
| 5/15/2014 9:53 PM | |
|
Posts: 12 Rating:
|
HelloMarcjan I have a question about the SFC59 which is the LADDR in SIMOCODE PRO V, DP Adresses or Imput's device? Right now i utilize DP adresses Your help is very importan for my project Regards Jose Colina Electrical Engineer
|
| 5/15/2014 10:29 PM | |
|
Joined: 5/28/2008 Last visit: 1/3/2026 Posts: 4522 Rating:
|
Hello, What impacy you mean in your question? LADDR is just an address. If you entered correct, you will get the correct values, if not then you may get wrong values from other device and address it in wrong field in HMI / SCADA or make wrong processing. Or you may put a value in LADDR not exist in the HW config, so you will get zeros. So, you have to put this value correctly. That's all. Hope this helps.
|
|
Ayman Elotaify |
|
This contribution was helpful to
|
|
| 5/15/2014 10:29 PM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Please read the manual related to the function, for LADDR you need a variable in word in Hex and you will find more if you check the file shared by MarcJan.It is start address of input/output that slave share with master on process image. Using slave address is wrong here.
|
Last edited by: hdhosseini at: 5/15/2014 10:35 PM// Ayman was faster |
|
This contribution was helpful to
|
|
Follow us on