(0)| 11/12/2013 2:14 PM | |
|
Joined: 1/28/2009 Last visit: 12/26/2025 Posts: 6887 Rating:
|
Hello, For S7 300/400 ,We can consider the bit inside the status word as special bits.They are activated on special occasions as explained in the manuals.If you have experience with smaller CPUs such as S7 200,There are special memories to indicate the first scan or memory for cyclic behaviors.These options are not available explicitly but can be created if necessary.Please, check the following discussion as a sample: Hamid Hosseini
power up bitI hope that helps |
Follow us on