(0)| 1/26/2016 11:58 AM | |
|
Joined: 1/28/2009 Last visit: 12/30/2025 Posts: 6891 Rating:
|
Hello , I hope I can help you by your application.Normally a SWR application is consisting of 2 CPU in different racks with a communication interface for redundancy data and a DP interface for process data communication with DP slaves.Please, try again by putting CPUs in different racks and assembling the rest of modules.Read more in the following manual: SIMATIC S7-300/S7-400 Software redundancy for SIMATIC S7 I hope it helps, hdhosseini |
| 1/26/2016 12:06 PM | |
|
Posts: 147 Rating:
|
Hello Hoseini Thank you so much, so that means that both cpus will have to have their own rails in the TIA selection tool? and are there any bus connectors required for each cpu? and how can we save space in the panel by having both CPUs on the same rail or rack?
|
| 1/26/2016 12:40 PM | |
|
Joined: 1/28/2009 Last visit: 12/30/2025 Posts: 6891 Rating:
|
so that means that both cpus will have to have their own rails in the TIA selection tool?
Yes , In your engineering software (STEP 7 or TIA Portal) , you need to use different racks. and are there any bus connectors required for each cpu? Yes , Keep the MPI connector for PG operation , Profibus connector for Master-->DP Slaves communications and if you use ethernet for communication between master and standby CPU , you need an extra ethernet connection. and how can we save space in the panel by having both CPUs on the same rail or rack? You can use the mounting rails with the dimension that suits your application.You can save space by using only essential modules on the main rack (PS,CPU,CP).Check width of each module and select the mounting rail you need from : SIMATIC S7-300 S7-300 Module data |
| 1/27/2016 7:52 PM | |
|
Joined: 1/28/2009 Last visit: 12/30/2025 Posts: 6891 Rating:
|
Thanks for your feedback, About the bus connectors that I was asking about it was regarding those small connectors that are inserted behind the CPU, IM, CP or I/O card, I should use a bus connector for both CPUs (one each?) About the bus connector, I meant the connectors for PROFIBUS or Ethernet.Check the following sample. And regarding redundant I/Os, would it work with IM 153-2 with software redundant S7-300 CPUs or are there anything different here? To answer to this question , please read the manual plus the following FAQ: Which modules can you use when implementing software redundancy? |
Last edited by: hdhosseini at: 1/27/2016 9:47:01 PM |
|
| 1/31/2016 10:45 AM | |
|
Posts: 147 Rating:
|
"if you use ethernet for communication between master and standby CPU , you need an extra ethernet connection." Can I use ethernet/profinet for software redundancy? the integrated port on an extra CP? |
| 2/1/2016 9:39 AM | |||||||||
|
Posts: 147 Rating:
|
so, can software redundancy be done in any way on ethernet/profinet? or MPI is the only option?
|
||||||||
Follow us on