5/31/2021 9:18 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1424)
|
Starting with STEP 7 V17, two new instructions for using S7-1500 in communication as OPC UA Client are available: OPC_UA_ReadList_C and OPC_UA_WriteList_C. These two blocks manage the establishment and finalization of connections, integrating in a single block what could before be done just by a set of blocks (OPC_UA_Connect, OPC_UA_NamesapceGetIndexList, OPC_UA_NodeGetHandleList, OPC_UA_NodeReleaseHandle, OPC_UA_Disconnect). In terms of usage, they are like OPC_UA_ReadList / OPC_UA_WriteList: just insert the block into the program, click on the toolbox and fill in the options. Tips:
Attached a sample project AttachmentOPC_UA_V17_20210531_1540.zip (1370 Downloads) |
Denilson Pegaia |
|
Follow us on