10/3/2016 11:28 AM | |
Joined: 2/27/2014 Last visit: 4/19/2024 Posts: 689 Rating: (199) |
Hello, Are you really want to control SINAMICS drive thru WinCC via OPC? If yes, then you should give detailed statement of your problem. 1st , you need to check the Drive can support OPC connectvity or not? Which Drive? Which connectvity?Which WInCC As per my knowledge SINAMIC S120 having data block structure like S7 PLC, so this drive can directly operate via WinCC or HMI via S7300/400 channel WinCC7.x or TIA WinCC Prof by default support OPC server/Client connectivity. I found one application note for OPC connectivity with S120 drive. In this case you need to define S120 drive as OPC server along with SIMATIC NET. Once its configure as OPC server then you can brows in WinCC under OPC channel. So WinCC will act as OPC client and drive will act as OPC server. If you feel this post is useful then don't forget to rate. Attachmentinfoplc_net_s120_opc.pdf (80 Downloads) |
With Best Regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on