4/8/2013 12:51 PM | |
Joined: 9/27/2006 Last visit: 4/18/2024 Posts: 12256 Rating: (2664) |
Hello Saggy; Since I cannot recognize the part number you are showing for your relay, it is difficult to give you straight information on the subject. And sincemost of myexperience with Siprotec relays lie with Profibus-DP communications, this is the bestinformation I can provide. First thing, remember that Siprotec relays are not a product of Siemens Automation and Drives (which hosts this forum), but is developped by another division, Siemens Energy. The divisions do not share ressources, so all information we can give you comes from the manuals they publish on the web. Start by having a look at various threads on Siprotec relays available on the forum: https://support.automation.siemens.com/WW/llisapi.dll?query=sipotec+profibus&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx%3Ftab%3D2&lang=en&siteid=csius&objaction=cssearch&searchinprim=_searchinprim_&nodeid=99&x=16&y=8&cssearchengine=NEW&x=0&y=0 Downloads of Profibus mappings ans gsd files for Siprotec relays. “Search Keywords” tab, language: English ,” Profibus” |
Last edited by: dchartier at: 8/28/2013 9:42 PM |
|
This contribution was helpful to1 thankful Users |
4/8/2013 4:05 PM | |
Joined: 11/8/2011 Last visit: 4/12/2024 Posts: 387 Rating: (43) |
thank you very much for you reply dchartier The relay part number i am using is 7SJ62 - 7SJ6231-5EB90-1FE4+L0A But in the link you sent iam not able to find GSD file Thanks in adavance |
Last edited by: Saggy at: 4/8/2013 4:11 PMLast edited by: Saggy at: 4/8/2013 4:11 PM |
|
4/8/2013 6:22 PM | |||
Joined: 9/27/2006 Last visit: 4/18/2024 Posts: 12256 Rating: (2664) |
Hello saggy; Try these links then: 6MD63, 7SJ61 / 62 / 63 / 64 Bus mapping (C53000-L1840-B006-03) V2.0_us GSD-File / GSD-Datei > V 3.00 All documents downloaded from: http://siemens.siprotec.de/download_neu/index_e.htm Hope this helps, |
||
Last edited by: dchartier at: 4/8/2013 6:27 PM |
|||
Follow us on