10/7/2016 2:43 PM | |
Joined: 8/3/2009 Last visit: 5/15/2024 Posts: 12951 Rating: (1650)
|
Hello Experts If you want to Install TIA Portal V14 on Real System or VM Ware you should renew your Windows Updates before. Look here is also a FAQ: https://support.industry.siemens.com/cs/ww/en/view/109739231 I have fallen into this trap. In a Test VM Ware it took very long (about more than 1 hour) (on a big Machine with SSD an a lot of RAM) then an error occurs because i have deactivated the Windows Update Service in the Win7 Services. Then second try: - install all current available Win7 Updates then the Installation of WInCC Prof V14 or Step7 Prof V14 took only about 25 min without Error. So be aware to fall also in this trap and ruin a lot of time. hope this helps Bye Murof |
Last edited by: Murof at: 10/7/2016 2:46:10 PMLast edited by: Murof at: 10/7/2016 3:05:43 PMIf this Information really helps, you could use the Rate function |
|
This contribution was helpful to5 thankful Users |
Follow us on