6/7/2010 10:35 AM | |
Posts: 19 Rating: (0) |
Dear experts I need analog output 0-10v at terminal 13 &14 (Micromaster440). Which parameters are to set for this application. Thanks Haque |
6/7/2010 11:49 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, You meant terminal 12 and 13. Look at attachment. Perhaps Operating Instructions (Compact): MICROMASTER 440 is useful. Best regards, Hristo Mihalev |
6/7/2010 1:05 PM | |
Posts: 19 Rating: (0) |
Dear UMENCHO Thanks for ur reply. Best regards Haque |
6/8/2010 8:40 AM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477) |
I am sorry but experts might have over looked your question. DIP Switches are for Analog Inputs not for Outputs For 0 to 10 V AO, you have to set 1 in P776 and set other parmetrs as suggested by RBM You must connect 500 Ohm resistor between Terminals 12&13 for AO1 and between 26&27 for AO2 Please Refer Parameter List manual for More details. Have a look to attached file Regards, Devesh AttachmentCopy of 440_PLi_23708204_en_0106.pdf (508 Downloads) |
Last edited by: Vithani at: 6/10/2010 11:02 AMI dnt mind if you give rate in addition to thanks....;) I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to3 thankful Users |
5/17/2016 11:27 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by sharif s is split to a separate thread with the subject Read the frequncy from drive. Best regards |
7/25/2017 6:59 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by yaseen.patel7 is split to a separate thread with the subject How to set 4-20ma current output from AO. Best regards |
Follow us on