4/5/2018 3:28 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425) |
Hi, The use of PN/PN Coupler is frequently used in communication between controllers that should have no direct connection. E.g. the configuration is simple, doesn’t require blocks call in user program. Attached, there is two casts that show how to configure it in TIA V15 when the controllers (S7-1200) are in a same project or when they are in different projects. TIPs:
References
Download de GSD
AttachmentPN PN coupler.zip (754 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to3 thankful Users |
Follow us on