10/16/2017 12:01 PM | |
Posts: 171 Rating: (44) |
Hi I have SIMATIC_CPU_1507S_V2_1.exe software downloaded from CPU 1500 . Windows 7 Ultimate SP1 64bit OS. Also there is no siemens sotware installed except latest prosave. While installing it's showing this error. Even I have sufficient space in requested drive. |
Last edited by: santhosh sundaram at: 10/16/2017 2:39:50 PMLast edited by: Jen_Moderator at: 11/17/2017 9:38:30 AMInserted right link. |
|
10/17/2017 12:04 PM | |
Joined: 5/12/2006 Last visit: 7/6/2024 Posts: 22299 Rating: (2996) |
Hello, from https://support.industry.siemens.com/cs/ww/en/view/109740725 Requirement for creation of a CPU volume The allocation and formatting of the CPU volume is carried out automatically during the installation process. One of the following requirements must be met for this: ● The partition style must be a "Master Boot Record (MBR)". You can find the partition style in the "Volumes" tab under "Computer Administration > Data storage medium management > Properties of the data storage medium". ● At least 401 MB of unpartitioned memory on the hard drive ● At least 401 MB available memory on the expanded partition on the hard drive ● At least 450 MB available memory on the unencrypted hard drive D:\\ Manual creation of the CPU volume If the CPU volume cannot be created automatically, you have the following options available: ● The installation process outputs a message that provides you the opportunity to manually perform the partitioning. Alternatively, you can cancel the installation process at any time. ● You must remove files from the D:\\ partition, since there is insufficient storage space available to perform the partitioning of the hard drive. ● You must manually decrypt the D:\\ partition
|
This contribution was helpful to1 thankful Users |
Follow us on