1/13/2012 8:41 PM | |
Joined: 6/4/2008 Last visit: 8/26/2024 Posts: 1495 Rating:
|
Hi, not much data to go on here. No description of what motor you want. Does it have a resolver built in? If you simply want to turn a motor to prove the hardware, then you can run an MC drive in open loop (without an encoder) to turn an induction motor. You don't need an OP1S as long as there is a PMU (Parameterising Unit) attached. I would recommend installing the Drivemonitor software - DownloadHERE See attached for cable details. If you want to run a synchronous motor, then you will probably need an encoder of some description. Regarding the parameterisation, I advise you follow the instructions in Sections 5 & 6 of theMC Compendium Best regards, Graeme AttachmentDrivemonitor_Cable.pdf (275 Downloads) |
Follow us on