6/25/2013 11:55 PM | |
Joined: 1/30/2009 Last visit: 7/26/2024 Posts: 18 Rating: (1) |
Graeme What is IVI and PSU cards? How can I diagnose these after CUVC board? |
6/26/2013 5:37 AM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477)
|
IVI is interfacing card - this card is used for interfacing control cicuit and power circuit PSU - is power card - this card gives power supply required by control circuit (24V) You can read more detailed description of hardware basics of master drive from following thread /tf/WW/en/Posts/21854 - And regarding your doubt about CU faulty or not - for that you can just try swapping CUVC from faulty drive to healthy - if fault is also swapped than CUVC faulty otherwise you need to check further Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on