(2)| 11/30/2010 10:01 AM | |
|
Joined: 4/14/2010 Last visit: 6/26/2025 Posts: 525 Rating:
|
GOOD AFTERNOON DEAR SIR I HAVE PROBLEM WITH DOWNLOADING CFC D7-SYS V7.0 PROGRAM UNFORTUNATELY I HAVE ONLY CARD CP5512 NO COM1 & COM2 IN MY PC HOW CAN I DOWNLOAD PROGRAM WHEN I COMPILE THE PROGRAM IT GIVE A MASSAGE LIBRARY UPDATES FILE (fbsgmc_fm1.a) HOW CAN I UPDATE MY LIBRARY KINDLY FIND ATTACHED SNAPS DEAR SIR IS THERE POSSIBILITY FOR DOWNLOAD PROGRAM WITH CP5512 MPI OR PROFIBUS.....? I AM TRYING TO DOWNLOAD VIA CPU MPI/DP PORT WHICH IS CONFIGUR ON PROFIBUS... CAN IT POSSIBLE TO DOWNLOAD PROGRAME ON DIRECT FM 458-1 DP THROUGH PORT X3 OR X1 WHICH INTERFACE REQUIRED..???? HOW CAN I UPDATE MY CFC LIBRARY...???? I AM STILL WAITING FOR YOUR ANSWER THANKS REGARDED AttachmentCFC V7.0.zip (911 Downloads) |
|
MS |
|
| 11/30/2010 10:45 AM | |
|
Joined: 8/25/2006 Last visit: 12/18/2025 Posts: 2221 Rating:
|
Hello. |
| 11/30/2010 2:10 PM | |
|
Joined: 4/14/2010 Last visit: 6/26/2025 Posts: 525 Rating:
|
THANK YOU SIR NOW I HAVE UPDATE NEW VERSION FILE LIBRARY BUT ONE FILE (FBAMAX) NOT IN INSTALLED LIBRARY HOW CAN I INSTALLED IT I HAVE ONLY TWO ERROR AFTER COMPILE THE PROGRAME FOR THIS FILE... WINDOW KINDLY CHECK ATTACHED.... I HAVE USB2.0 TO RS232 SERIAL INTERFACE CONVERTER WITH THIS CABLE DB9 PIN CONFIGURATION MAIL-FEMAIL DB 9 PIN ASSIGNMENT (2-3 , 3-2 , 5-5) CAN IT POSSIBLE TO DOWNLOAD PROGRAM IN FM 458-1 THROUGH X1 PORT..??? THANKS REGARDED AttachmentCFC NEW VERSION.zip (876 Downloads) |
|
MS |
|
| 12/1/2010 11:05 AM | |
|
Joined: 8/25/2006 Last visit: 12/18/2025 Posts: 2221 Rating:
|
If you know how works the blocks from FBAMAX you can try to replace them with blocks from standard library.
You can, if you know how works the existing blocks.
All manuals for FM458 available here.
The reason is that you still did not load program to the FM.
You can load offline only using Simatic Field PG or external Simatic USB-Prommer.
After successfull compiling it will be possible to load online. No. |
| 12/1/2010 12:49 PM | |
|
Joined: 8/25/2006 Last visit: 12/18/2025 Posts: 2221 Rating:
|
If you have compiled program you may load it offline, but to ensure the correct work I think you need to have installed the same software versions as were installed on PC where the program was compiled. And after loading you may work but not so long. Some day, when you will need to change something in the program you will need again FBAMAX to compile and download program with changes. Field PG M3and USB-Prommer. |
Follow us on