(0)| 9/30/2014 1:43 PM | |||
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello K,C,; Could you explain what you intend to do with this type of information? You do realise that performance data such as you are asking for cannot be taken out of a hat. It is highly dependent on the installed software, OS and environment, hardware and software versions, network interfaces and switches...It is somewhat like purchasing a new car based on the fuel consumption data provided by the vendor: it is highly unrealistic to believe you can ever achieve that kind of mileage to fuel ratio in real life. To start the discussion: Look at the pdf document provided by member BilalD in the following discussion on a similar subject: Performance data document WinCC V7 - Siemens As far as NTP synchronization is concerned, maybe you can find your answers in the following collection of FAQs: Time synchronization - Time synchronization in the automation environment Use the NTP button on that link to get to the specific FAQs and applications on WinCC and Time synchronization. For example:
Hope this helps, Daniel Chartier
|
||
Last edited by: dchartier at: 10/1/2014 4:18 PM |
|||
Follow us on