(0)| 11/8/2014 1:21 PM | |
|
Joined: 3/22/2014 Last visit: 5/27/2024 Posts: 2 Rating:
|
Dear sir, I was commissioning one labeling machine which is equiped with s7-200 smart cpu with sinamics v90 drive. I want to instant stop my servo when one input comes. But I am facing problem that my lable goes 3 or 4 mm ahead instead of stoping when my input comes. my ramp down time is 0 second, decceleration time 20 ms. I have used motion wizard in s7-200 smart. I have already tried stp input in wizard. I have also tried using hardware intterupt.Besides all these thing I have tried to change the mode of v90 in running condition.
-------------- New subject after splitting from know what the software to operate the simatic s7 200 smart (cpu st40). |
Last edited by: Min_Moderator at: 11/10/2014 12:00 PMSplitted |
|
| 5/8/2015 2:15 PM | |
|
Joined: 5/6/2015 Last visit: 11/5/2025 Posts: 43 Rating:
|
Hello, Is this still an issue for you? |
| 8/21/2015 1:19 PM | |
|
Posts: 3 Rating:
|
the input which is coming to plc is having some delay, it may be because of that . |
| 12/16/2015 2:40 PM | |
|
Posts: 4757 Rating:
|
New question published by Davinder Singh is split to a separate thread with the subject Sample program to control v90 servo with s7 200 smart. Best regards |
Follow us on