(0)| 12/10/2014 9:47 PM | |
|
Posts: 5 Rating:
|
secondly i also need help configuring ET200L profibus with plc 314 2pndp my question is, should i need configure both ET200L and terminal box TB32L because i cannot find any hardware configuration for TB32L and in my input adresses and out put adresses it says that it start from 0 to 2046 which i think is not noral, i would be thankful for kind information. --- Thefirst question in this post islocated in the thread Looking for Hardware configuration for micromaster 420. --- |
Last edited by: Min_Moderator at: 12/11/2014 9:16 AMLast edited by: Min_Moderator at: 12/11/2014 9:11 AMSplitted |
|
| 12/11/2014 2:31 AM | |||||||||||
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello muhammad; The MM4 drive is not part of a S7 PLC, so it has no hardware configuration in Step 7. Unless you intend to communicate with it over Profibus. Then you have to set the gsd file for the Profibus communication module (6SE6400-1PB00-0AA0)in the Profibus configurator. Getting Started Guide PROFIBUS Module Operating Instructions: MICROMASTER PROFIBUS Optional Board As far as the ET 200L,I know ita brick-style slave, in definite I/O sizes, without terminals to be configured. For example:
Could you tell us the part number of the unit you want to configure? Hope this helps, Daniel Chartier |
||||||||||
Last edited by: dchartier at: 12/11/2014 3:07 AM |
|||||||||||
This contribution was helpful to
|
|||||||||||
| 12/11/2014 4:00 PM | |
|
Posts: 4620 Rating:
|
Hello muhammad sohaib iqbal, What you're talking about is the terminal block of the ET200L has nothing to do with the hardware configuration, you have to read the code of the electronic module, e.g.: if you have the electronic module 6ES7 131-1BL12-0XB0 which is a unit 32 digital inputs expandable with modules SIMATIC SC, you can find in the hardware catalog under PROFIBUS, choose the folder ET200L and you will find the description L SC-DI 32x24DC. |
Last edited by: Ste39 at: 12/11/2014 9:17 PMLast edited by: Min_Moderator at: 12/11/2014 4:15 PMDelete empty quotation |
|
Follow us on