(2)| 1/19/2015 3:55 PM | |
|
Posts: 6 Rating:
|
Hello all, We have a 414 PLC type "6ES7 414-2XK05-0AB0". It does not go to run mode with the program or with only OB1. We tried to MRES and download an empty program only OB1. But it does not run anyway. "It is saying STOP due to IO error ". But no IO module is used to check also if there is something wrong. I am totaly confused. So, what could be the reason for this issue? I attached the Diagnose.txt. Maybe you can help me to find a way. Thanks in advance! best regards Mustafa AttachmentDiagnose.zip (1086 Downloads) |
| 1/19/2015 5:31 PM | |
|
Posts: 6 Rating:
|
I am continue to trying. First of all I discard the memory card. I made a memory reset. And then I have loaded the OBs 80-82 , OB84-86, OB100, OB121-122 as empty. And I restart the PLC. Then it is already in stop mode. Not possible to make start. I put two screen shot. Maybe they would be helpful to define possibilities. Thanks in advance! Best regards. Mustafa AttachmentScreenshots.zip (1113 Downloads) |
| 1/19/2015 6:15 PM | |
|
Posts: 6 Rating:
|
the link is not opening! Could you please check it? Thanks MicroMan |
| 1/19/2015 6:29 PM | |
|
Posts: 6 Rating:
|
When I copied the link to address bar, it was opened. So that means the CPU defected? :( |
Follow us on