(0)| 3/4/2015 2:14 AM | |
|
Posts: 1 Rating:
|
Dear All, I have used an old program which has the PLC program and HMI integrated together for migration. I only woul like to change the old touch pnel from TP177B to TP700 but all PLC remain the same. I have migrate only the HMI to TIA . I will load the HMI using TIA and the PLC using Siemens Simatic. Will these work??? or do I need to migrate both the PLC software and the HMI to TIA then it will work???
------------- |
Last edited by: Min_Moderator at: 3/4/2015 1:11:19 PMNew subject after splitting |
|
| 3/4/2015 5:49 PM | |
|
Joined: 5/12/2006 Last visit: 1/21/2026 Posts: 22829 Rating:
|
Hello, yes is possible to migrate the HMI only. For the usecase PLC in Step7 V5.x and HMI in TIA there a few guidelines: Here you find a overwiew combined configuration in this document you find a explanation for the device proxy Regards Christoph |
Follow us on