(1)| 3/27/2015 10:13 AM | |
|
Posts: 42 Rating:
|
Hello freinds.. i also use the HSC in the s7-200 smart PLC. i know that the SMD38 is the ACC and the SMD48 is the PRESET value.but i have some query about it that are below.. 1) up to how much maximum count the HSC can count?? 2) if i give the any preset value to SMD48 and when it reached the interrupt is generated but how the value of the SMD38 is reset. is there any script which i have to write in the HSC subroutine.. There are the screenshot of my program is attached....
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 3/27/2015 11:58:24 AMNew subject after splitting |
|
| 3/27/2015 1:29 PM | |
|
Posts: 42 Rating:
|
Thanks for your reply dear... i hope it will definetely help me... Thanks again dear... |
| 6/19/2017 5:38 PM | |
|
Posts: 4757 Rating:
|
New question published by Amy1 is split to a separate thread with the subject Smart 200 PLC with 4 Encoders of A phase. Best regards |
Follow us on