4/29/2015 8:58 PM | |
Joined: 11/19/2011 Last visit: 10/11/2024 Posts: 88 Rating:
|
hello after powring up the plc the only led DCV5 and STOP led are ON the problem is that the cpu runs normally when i put the switch on STOP mode and swich it back on RUN mode(manual start). but if i switch off the entire machine and switch it on the cpu goes into STop mode . the cpu is connected to a slave DP (wago i/o module) when i logged to diagnostic buffer it shows that the cpu requests a manual warm restart ( the diagnostic buffer is attached) AttachmentDiagnose.txt (723 Downloads) |
4/30/2015 12:03 AM | |
Joined: 11/19/2011 Last visit: 10/11/2024 Posts: 88 Rating:
|
i had this problem with the ob 86 loaded |
Last edited by: sukhoi at: 4/30/2015 12:04:04 AM |
|
5/4/2015 11:08 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
|
5/26/2015 9:06 PM | |
Joined: 11/19/2011 Last visit: 10/11/2024 Posts: 88 Rating:
|
hello i did a diagnostic in stop mode and run mode and with a new program with OB1 only Attachmentdiagnose in stop.txt (695 Downloads) |
5/26/2015 9:08 PM | |
Joined: 11/19/2011 Last visit: 10/11/2024 Posts: 88 Rating:
|
this th empty program
Attachmentempty.txt (744 Downloads) |
5/26/2015 9:10 PM | |
Joined: 11/19/2011 Last visit: 10/11/2024 Posts: 88 Rating:
|
this in run mode , i think the problem comes from thz memory card because in the empty program the cpu request a reset of the mmc ?
Attachmentrun mode.txt (816 Downloads) |
Follow us on