(0)| 5/1/2015 4:40 PM | |
|
Posts: 2 Rating:
|
I am getting this same error but I am using TIA Portal V13 SP1. This has worked for the last few weeks with no issue. Now I cannot get online with my PLC very suddenly. I am running Windows 7 Pro, 64bit. Last week I was forced to accept a few Windows updates... perhaps that is the issue. Please help!
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 5/4/2015 3:19:30 PMNew subject after splitting |
|
| 5/4/2015 3:39 PM | |
|
Joined: 5/12/2006 Last visit: 1/19/2026 Posts: 22829 Rating:
|
Hello,
with which interface you would go online ? ETHERNET?MPI?PROFINET?
Regards |
| 5/6/2015 8:48 PM | |
|
Joined: 7/7/2010 Last visit: 1/16/2026 Posts: 16379 Rating:
|
Keep track of the updates installed since communications last worked. Revert to the prior version of whatever was patched (uninstall update) and try until you isolate which windows update caused the problem. Now report this to Siemens support. Lastly, put a post-it note on your computer with the update you need to avoid installing until portal is fixed to allow that update. If that does not fix the problem, was any other software installed or updated in the meantime?
|
Last edited by: huggy_d1 at: 5/6/2015 8:50:16 PMscience guy |
|
| 5/31/2016 2:07 PM | |
|
Joined: 8/4/2015 Last visit: 9/11/2024 Posts: 7 Rating:
|
Hello, I am sorry for refreshing old thread but it looks like I have similar or the same problem like an author. So far I was using TIA portal V12 and I've never had any problem with communication. Lately I uninstaled TIA V12 and installed TIA portal V13 SP1. When I tried to connect with my new PLC in new TIA I noticed that I am not able to choose my local ethernet card in show accesible device function. I only can choose Teleservice option. What is interesting I can see my local ethernet card in menu online access and when I am clicking update accessible devices there, I get an error in message window: Online: Function not implemented in loaded communication driver. Moreover I am able to ping my PLC from command window. My system is win 7 64 bit. I am also sending some screens from my computer in doc file. Could you please help me to find solution for this problem? Thank you in advance, Rafal AttachmentDok1.docx (483 Downloads) |
| 4/27/2020 9:26 AM | |
|
Posts: 4 Rating:
|
Hello friend. I am also facing the same thing. IP was ping but cpu not accessible. . From where you changed PN/ie. |
Follow us on