(0)| 6/1/2015 9:17 AM | |
|
Posts: 462 Rating:
|
Hello All, I want to connect MM420 ( 6SE6420-2AB22-2BA ) to S7-1500 with STEP7 V13. But i can not find the MM420 GSD file. Please help me. Thanks a lot |
| 6/1/2015 6:42 PM | |
|
Posts: 462 Rating:
|
Hello I need the gsd file for MicroMaster420. i could not find that yet. Can everyone please help me? |
| 6/1/2015 8:24 PM | |
|
Joined: 9/27/2006 Last visit: 1/13/2026 Posts: 12480 Rating:
|
Hello tekabi; In this recent thread you include screencaptures that show the MM4 Profibus option board as part of the Profibus catalog of your CPU. You would not need to insert the MM4 Profibus option board in the HWConfig if this is the case, it ios already in the gsd directory. If however you need to insert the MM4 Profibus Option board (MFLB: 6SE6400-1PB00-0AA0) in the Profibus configurator of a third-party PLC, you could find it here (as a zipped file): MICROMASTER 4: Amended PROFIBUS GSD files (inc. MICROMASTER 411, 420, 430 und 440) Information on basic parameters and programminginstructions can be found here:
Getting Started Guide PROFIBUS Module
Operating Instructions: MICROMASTER PROFIBUS Optional Board Hope this helps, Daniel Chartier
|
Last edited by: dchartier at: 6/1/2015 8:29:07 PM |
|
Follow us on