(2)| 6/2/2015 10:05 PM | |
|
Posts: 108 Rating:
|
Hi I have a smiliar problem if i wanna simulate a V3.0 or below. If they dont allow you to simulate it in PLCSim V13, where can you simulate them? ------------ |
Last edited by: CS Moderator at: 6/3/2015 11:40:13 AMsplitting |
|
| 6/2/2015 11:58 PM | |
|
Posts: 108 Rating:
|
Oh, ok thanks, in that way, i'll use only V4.0, coz i'd tried to use the PID on this CPU for a test. Btw, may you check this problem? [snip] ...
------------- |
Last edited by: Jav Pinz at: 6/3/2015 12:23:45 AMLast edited by: CS Moderator at: 6/3/2015 12:02:27 PM |
|
| 6/8/2015 10:42 AM | ||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Posts: 30 Rating:
|
hi Christoph , i tried like you say first open a new project and then open the PLCSIM . The tia V13 SP1 didn't recocnize the PLC SIM. The PLCSIM didnt show any IP Address after a a new project from PLCSIM was created. I try to Repair the software by installing the PLCSIM again, it doesnt help... what should i do now? SP1 Doesn't work , why? This software component is what i have and installed on my PC.
i attached a file with the error that PLCSIM was created. Attachment1ceca7aa-c30b-4bd3-ab38-df80722b2a2e.zip (461 Downloads) |
|||||||||||||||||||||||||||||||||||||||||||||||||||
| 6/8/2015 12:53 PM | |
|
Joined: 5/12/2006 Last visit: 1/12/2026 Posts: 22818 Rating:
|
Gi,
have you start PLCSIM from inside TIA Portal or external? Christoph |
| 6/8/2015 3:25 PM | |
|
Posts: 30 Rating:
|
yes i tried to do that , look at the attachement |
Follow us on