(0)| 6/10/2015 12:57 PM | |
|
Posts: 3 Rating:
|
This worked pretty well for me, EXCEPT: When I have two languages in the program, and I give them different font sizes, they both show up the same size. (For example, I set English to font size 21, and French to font size 16. However, if I access the password screen in English, then later in French, the text is shown in font size 21 in both occasions). This is a problem because the French words are longer, and hence some letters get cut off. Any ideas about how to get around this? (besides just using font size 15 for both?)
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/10/2015 4:08:55 PMNew subject after splitting |
|
| 6/10/2015 4:11 PM | |
|
Posts: 4757 Rating:
|
|
Follow us on