(0)| 6/14/2015 2:04 PM | |
|
Posts: 2 Rating:
|
I just purchased a new micromaster 420 vfd and I am unable to communicate between my laptop and the vfd. The other VFD's are version h01/2.21 and the , DriveMon is V5.4+SP2. I am trying to communicate via Micromaster /PC inverter connection kit (6SE6400-1PC00-0AA0). When i search for the drive in the "establish USS connection, It shows the drive but not what version it is. Do I need to update my DriveMon program? I have attached the my DriveMonitor, New MM420 Drive and DriveMonitor version in xlsx file.
---------------------------------------------------------------------------------------------------- AttachmentBook11.xlsx (534 Downloads) |
Last edited by: manojchand123 at: 6/14/2015 3:37:46 PMLast edited by: manojchand123 at: 6/14/2015 3:38:35 PMLast edited by: Min_Moderator at: 6/15/2015 3:11:01 PMNew subject after splitting |
|
| 6/16/2015 9:25 AM | |
|
Posts: 4620 Rating:
|
Hello manojchand123, I think you need STARTER, Have a look: Micromaster 440 V 2.2 firmware connection with Drive Monitor ...
|
Follow us on