(0)| 7/2/2015 2:32 PM | |
|
Posts: 2 Rating:
|
Can Anyone tell me if the ET200S 6es7 151-1aa02-0ab0 is compatible with TIA. I am having a hard time finding the GSE.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/2/2015 3:53:36 PMNew subject after splitting |
|
| 7/2/2015 2:56 PM | |
|
Joined: 5/12/2006 Last visit: 1/22/2026 Posts: 22807 Rating:
|
Hello,
this Interfacemodule is not supported in the HW Catalog of TIA, is to old. The GSD File you can download here: https://support.industry.siemens.com/cs/ww/en/view/652154 Regards Christoph |
| 3/11/2021 10:23 PM | |
|
Joined: 7/6/2015 Last visit: 12/27/2024 Posts: 1 Rating:
|
Hi ChristophD, Do you know if I can use a 6ES7 151-1AA02-0AB0 but in TIA configure it as 6ES7 151-1AA04-0AB0, would that work? Is the IM151-1AA0x_Std-CU.ZIP for configuring the older module like the 1AA02 in TIA? Reason I am asking is we need to use about 10 of these on a project, if I use the 1AA0x I can't seem to pack address for 4DI cards, but if I configure it with the built in 1AA04 then I can pack addresses. Thanks in advance. Allen |
Follow us on