(0)| 7/29/2015 8:38 AM | |
|
Joined: 4/24/2006 Last visit: 1/9/2026 Posts: 9104 Rating:
|
Hello, Try to reset the CPU to "reset in the as delivered state", Have a look at the following link: how do you reset a SIMATIC S7-300 CPU and MMC (default reset or overall reset)? Best regards, Wizard |
| 7/30/2015 4:02 PM | |
|
Posts: 31 Rating:
|
I just did that. The name and IP address were removed. I then assigned an IP through the 'Edit Ethernet Node' in HW config but when I try to connect/download it now says "Connection Could not be established. The connection Partner is not responding" Did I do anything wrong?? |
Follow us on