(0)| 8/10/2015 4:49 AM | |
|
Joined: 4/28/2015 Last visit: 4/8/2025 Posts: 1 Rating:
|
Hi everyone. I have a CPU 315 2PN-DP with a TP1200 touch panel in a small profinet network. When i look for accessibles nodes in TIA portal v13 or step7 2010 both find all the devices. But when i connect this small network to a bigger one (almost 60 devices), i can not find any devices. Strange thing is i can ping to any devices, and they answer. Is there any timeout parameter or something like that i need to increase? because my problem is not to found any device trough the "accessible nodes" function. My problem is that one device is not reachable by the CPU 315. So it shows the red cross icon. Thanks.
---------------------------------------------------------------------------------------------------- |
Last edited by: AutoGen_934851 at: 8/10/2015 4:54:05 AMLast edited by: AutoGen_934851 at: 8/10/2015 4:54:53 AMLast edited by: Min_Moderator at: 8/10/2015 10:13:12 AMNew subject after splitting |
|
| 8/10/2015 11:25 AM | |
|
Joined: 12/16/2012 Last visit: 9/8/2025 Posts: 655 Rating:
|
Hi! Sounds like they are not in the same subnet (same IP address, except last number). |
Follow us on