(0)| 8/24/2015 7:00 PM | |
|
Posts: 4 Rating:
|
Hello There; In my work machine, I have a ıpc427.When I wrote the PCs IP address, a screen asking the user turns against my username and password.here, as in Simotion Fixed (if changed) transaxle can enter a password and user name. for example simotıons in, we scan the screen, type the IP code the user name and the password line "simotions" is enough to write.This way, you can monitor the values as the machine's control panel simotıons the status of other drives and axis angle.the same situation applies in ıpc427c? for example, Simotion web page opens when we entered the IP number.There are pictures in the attached file.such as user name and password here "simotions" Simply write.microbox similar situation applies for machines using the IPC.IPs only written document on the IPC or machine identity number, user name and password once you opened transaxle can enter our page?Thank you in advance for your response. Attachmentsımotıon web page.docx (362 Downloads) |
Last edited by: ugurs at: 8/24/2015 7:16:10 PM |
|
Follow us on