(1)| 8/25/2015 10:28 AM | |
|
Posts: 2 Rating:
|
Is it possible to communicate between S7-200 SMART and S7-400 over profinet? If possible, please provide a reference. |
| 8/25/2015 11:05 AM | |
|
Posts: 5521 Rating:
|
hi DGhosh, for Profinet, one of them should be device to the other. As I know S7-200 don´t supports Profinet. but I think there is a possibility to do it just over Ethernet. For this see following FAQ: How do you configure an S7 connection for data communication between an S7-200 and an S7-300 or S7-400 on the Industrial Ethernet?hope this helps,regards, |
| 8/25/2015 11:52 AM | |
|
Posts: 5225 Rating:
|
As background information only. |
Last edited by: Min_Moderator at: 8/25/2015 1:30:40 PMPicture -> Attachment |
|
| 8/25/2015 1:58 PM | |
|
Posts: 5225 Rating:
|
DGhosh - There is a problem with my earlier notes. I have looked through the System Manual for the S7-200 Smart (A5E03822230-AB). I cannot confirm that the built-in Ethernet port is in actual fact a Profinet enabled port. I would assume as much as there is mention of Put and Get functions in the manual under the heading of "7.3.1 Get table and put table (Ethernet)". There is also special mentions in the updated text document found under [LINK]. It may very easily be that the S7-200 SMART can link with the S7-400, but that this fact is not publicly mentioned anywhere... it is really best to contact your nearest Siemens distributor or perhaps.. |
Last edited by: William_B at: 8/25/2015 1:58:49 PM |
|
This contribution was helpful to
|
|
| 3/27/2018 3:21 PM | |
|
Joined: 8/21/2014 Last visit: 1/20/2026 Posts: 1098 Rating:
|
New question published by Pravin12345 is split to a separate thread with the subject communication issue of S7 200 Smart PLC with PLC S7-410 Over Profibus. Best regards |
|
My Forum is the place to personalize your profile, |
|
Follow us on