9/23/2015 2:17 PM | |
Joined: 5/17/2010 Last visit: 8/20/2025 Posts: 226 Rating:
|
Hi, In my opinion this should work with Win-SIMOCODE-DP Professional software. As I know this PC-Adapter does not need 24V DC supply out of the PROFIBUS device interface, just 5V via USB. The older PC-Adapter was powered by 24V DC out of PROFIBUS interface or via external supply. SIMOCODE devices do not supply 24V at the PROFIBUS interface. Would be nice to get a feedback of you.
Best Regards
|
------------------------------------------------------------------------------------------------ |
|
12/23/2015 1:58 PM | |
Joined: 5/28/2015 Last visit: 7/30/2025 Posts: 24 Rating:
|
Hi Use Profibus DP and the Simocode ES. |
2/26/2016 1:07 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
New question published by MacMbi is split to a separate thread with the subject Change any parameter via the CP5512 interface, Error when SIMOCODE not running. Best regards |
Follow us on