(3)| 9/22/2015 6:35 PM | |
|
Posts: 23 Rating:
|
I have a similar problem here. We have windows 7 64 bits and microwin 4.0 SP9. The software runs ok, but we can not download the program to the PLC. In the set interface PG/PC we selected option Microwin-> PC/PPI but in local connection we only have the usb option and there aren't COM ports to select. The computer have two serial ports. I also tried to use a USB/Rs232 conversor that generates another COM port in the device manager but I can't choose this option, USB is the only option in the combo box. Any suggestions are welcome ------------------------------------------------------------------------------------------ |
Last edited by: miguel_lopez at: 9/22/2015 6:35:56 PMLast edited by: miguel_lopez at: 9/23/2015 10:47:07 AMLast edited by: Min_Moderator at: 9/23/2015 1:29:50 PMNew subject after splitting |
|
Follow us on