(0)| 10/1/2015 8:32 AM | |
|
Posts: 4 Rating:
|
Hello, I have an issue of no alarm message/description being displayed on HMI Alarm View for an acknowledged alarm. My application uses PLC alarms instead of HMI alarms and is developed using Simatic TIA Portal v13 SP1. To generate and ackowledged an alarm, the following instruction (in SCL language) is used: #T_nRetVal := ALARM_DQ(SIG := #Alarm_Status, ID := W#16#EEEE, EV_ID := #Event_ID, CMP_ID := W#16#0001, SD := #Tag_Index); #T_nRetVal := ALARM_SC(EV_ID := #Event_ID, STATE => #Ret_Val_State, Q_STATE => #Ret_Val_Q_State); For triggered alarms, I can get the relevant alarm message on HMI Alarm View for incoming or outgoing alarms, but no alarm message is displayed for acknowledged alarms. Instead of re-creating all alarms as HMI alarms, I would like to know whether there are some ways to resolve this issue or perhaps other PLC instruction(s) or different way to program it. Any suggestion is highly appreciated. Thanks. Sony ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/1/2015 9:33:38 AMNew subject after splitting |
|
| 10/1/2015 10:14 AM | |
|
Posts: 4757 Rating:
|
Closed cause question posted twice. The second thread with the subject Non-displayed alarm messages on HMI Alarm View is published within the conference STEP 7 (TIA Portal). Best regards Min_Moderator |
Follow us on