(2)| 10/26/2015 8:55 AM | |
|
Posts: 5521 Rating:
|
hi David, DP/DP-Coupler is easy. you have to project it on each side as slave with the transfer-areas that you need. When you have e.g. 16 Byte Input on the one side in slot 1 you need 16 Byte Output on the other side in slot one. Maybe the manual could help you: DP/DP Couplerhope this helps, regards, |
| 10/26/2015 9:15 AM | |
|
Posts: 767 Rating:
|
Do I need to add the coupler in ABB side as well?
|
| 10/26/2015 9:53 AM | |
|
Posts: 5521 Rating:
|
Yes, project it on each side. here you find the GSD-Files: PROFIBUS GSD files : LINKhope this helps, regards, |
| 10/26/2015 10:00 AM | |
|
Posts: 767 Rating:
|
Thanks a million. One more question: do I need to add the ABB controller in simatic manager as well? I'm new in this, that's why I ask these questions. Regards
|
Follow us on