(0)| 11/26/2015 5:48 AM | |
|
Posts: 7 Rating:
|
oh sorry the attachment is here, |
| 11/26/2015 8:59 AM | |
|
Posts: 4620 Rating:
|
oh sorry the attachment is here, ashulogo8 wrote: Hi the logo cable has logo plc written on it pls see the attached image, should i return it back (if it is useless---means i can not use it with my 0BA8 logo)
Hello, you're in the same school? |
| 11/26/2015 7:21 PM | |
|
Posts: 7 Rating:
|
Hi thanks all for instant reply, actually my problem is something different, I have purchased the logo cable from ebay, at that time i did'nt know anything about PLCs, my project guide told me "just buy a logo plc and its programming cable" and I bought the cable first becoz logo plc was not avail. at that day. but when the cable came surfing net about its drivers i found that the new version logo8 does not require that cable, from the ashulogo8's post i came to know that even there is no port to connect the usb logo cable. I met ashulogo8 in my VLSI lab. he is also worried about purchasing the cable, i picked up the cable image from his post and attached in my post as at the time of posting i was in hurry.
option 1 : throw my USB logo cable in waste basket, as ebay is not ready to return it option 2 : do not buy the newest version of logo (i.e., logo 8) but buy an old version of Logo plc which can be programmed by using my logo cable so that my investment in logo cable will not waste. I can't throw it in waste as i bought it by my pocket money, I am therefore asking you please tell me which versions of logo plcs support my usb logo cable ------- i will buy only that logo plc which can be programmed by using my logo cable to make my logo usb cable in working and useful. My work is only a switch on/ off some motors depending upon the logic / switches ---- not require advanced dataloging or webserver etc
some venders are offering me logo 0ba2 the images are also attached
i will show you any image of logo plc before ordering it to make sure this time i should not make a mistake.
thanks in advance Attachmentimages.pdf (1454 Downloads) |
| 11/27/2015 9:22 AM | |
|
Posts: 4757 Rating:
|
New question published by sth411 is split to a separate thread with the subject Logo8, how do I set the ip-address?. Best regards |
| 11/27/2015 6:34 PM | |
|
Posts: 7 Rating:
|
actually i can get the older versions from some sellers but is it sure 0ba2 is programable with my cable thanks |
Follow us on