(0)| 12/18/2015 11:12 AM | |
|
Joined: 4/9/2013 Last visit: 9/29/2025 Posts: 26 Rating:
|
Hi all, I also have a problem with my SF red LED witch is ON now. I've checked the diagnostic buffer but everything is ok there. The CPU is in RUN mode. I have compared all the offline/online blocks and the result was: "Blocks are identical". The Hardware Config is also ok.(all devices green in online mode) I'm using S7-314C and TIA Portal V13 SP1. What can be the problem? ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 12/18/2015 3:53:18 PMNew subject after splitting |
|
| 12/18/2015 4:22 PM | |
|
Joined: 5/12/2006 Last visit: 1/23/2026 Posts: 22831 Rating:
|
Hello, have you a screenschot of the Deviceview of the PLC in Online mode? Christoph |
| 12/20/2015 1:06 AM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Dear Razvansql, Please update your software, update 6 is already available. Updates for STEP 7 V13 SP1 and WinCC V13 SP1 If there are no diagnostic errors in the diagnostic buffer then it might be the firmware version and/or the TAIP software. |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on