(0)| 12/23/2015 2:52 PM | |
|
Posts: 35 Rating:
|
Hi guys, The attachment file is the picture I print screen. My HMI model is TP1200. What happened before. 1. I download the program to the HMI 2. After it's done, the start button on the HMI cant be press 3. So I tried to restart the HMI by switch on and off the cycle power 4. After power up the white screen asking for OS update is appear. Before this I can download the program inside and it works. Question 1. From the picture no 2, why the step no 4 is asking to switch off the power supply of the operator panel (HMI)? 2. After I switch off, do I need to switch back to on? 3. From picture no 3, I did follow the step but I could not proceed to the Load. I am using the ethernet protocol. I using the default IP address : 192.168.0.2 but could not connect and the load button did not appear. 4. I tried to skip step 6(pic no 3) but I could not establish the connection. Thank you. AttachmentPIc.rar (1111 Downloads) |
| 12/23/2015 2:53 PM | |
|
Posts: 35 Rating:
|
Hi guys, The attachment is for the question up there. Thank you. AttachmentPic2 & manual.rar (1346 Downloads) |
Follow us on