(0)| 1/14/2016 4:35 PM | |
|
Posts: 13 Rating:
|
Hi We have an Servomotor with sinamics S120 servo drive. that connected to a S7-1500 PLC by Profinet. The application is Perforating of lable films with special length and print mark references. I connected print mark to the S120 and I want to use it to stop the film in same position in each cycle Perforating it and move again to next step. Perforating motor has a separate mechanism that goes up and down. How can I use the print mark that I connected to drive input to receive to accurate stopping in same positions. Is there any simple solution. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/15/2016 11:43:07 AMNew subject after splitting |
|
Follow us on