(6)| 1/16/2016 9:45 PM | |
|
Posts: 3 Rating:
|
So this mean only works with Win XP? |
| 10/26/2017 2:13 PM | |
|
Joined: 7/9/2015 Last visit: 1/9/2026 Posts: 2 Rating:
|
Buon giorno,vorrei condividere la seguente informazione.Da tempo cerco di far girare Step7 Microwin con Windows10.Sino ad ora ero riuscivo a installare la versione4.0925 di MicroWin,ma non riuscivo a comunicare con il PLC perché non si riusciva a impostare l'interfaccia di comunicazione;praticamente aprendo l'interfacciaPG/PCnon si potevano scegliere le interfacce per comunicare, semplicemente perché non erano presenti,ed ero costretto a girare con due PC con sistema operativo diverso.Per risolvere il problema basta scaricare da Siemens la versioneTrial di Step7 versione 5.6ed installarla suWindows10,l'installazione diStep7 v5.6,sovrascrive tutto quello che serve perl'interfaccia PG/PC. Adesso si possono scegliere le interfacce conMicrowin, ed andare finalmente on line con ilPLC S7200. Good morning, I would like to share the following information. For a while I try to run Step7 Microwin with Windows10. So far I was installing version 4.0925 of MicroWin, but I could not communicate with the PLC because I could not set the ' communication interface, practically opening the PC / PC interface, you could not choose interfaces to communicate, simply because they were not present, and I had to run with two PCs with different operating systems. To solve the problem just download Siemens from Step7 trial version version 5.6 and install it on Windows10; the installation of Step7 v5.6 overwrites everything you need for the PG / PC interface. Now you can choose interfaces with Microwin, and finally go online with the PLC S7-200. AttachmentStep7Microwin_Windows10.pdf (5881 Downloads) |
Last edited by: Calderaro at: 10/27/2017 12:46:25 PMLast edited by: Calderaro at: 10/27/2017 12:51:14 PM |
|
This contribution was helpful to
|
|
Follow us on