(4)| 1/19/2016 7:59 AM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello, Can you tell us if this project originally was created using Protool (OP7) and then migrated to WinCC flexible (OP77A)? If yes, then the cause of this problem is because you have created the project using WinCC fle3xible 2008 SP2 "which is mentioned in the device connection in Step7 program". And then may be somebody edited the project using SP3. To Avoid installation of SP3, You can ask anybody who have WinCC flexible SP3 to open the project and then do the following steps: Go to Project / Save as Version and then select WinCC flexible 2008 SP2. Then he can give you the saved project and then you can open using SP2 I know that lot of users prefer to use SP2 than SP3 because you can open and migrate protool project with SP2 and this feature is not available in SP3. If all of the above is not your case, then try to do one of the following steps:
Hope this helps. |
|
Ayman Elotaify |
|
| 1/19/2016 9:27 AM | |
|
Joined: 5/12/2006 Last visit: 1/19/2026 Posts: 22829 Rating:
|
WinCC flexible 2008 SP3 can downloaded here: https://support.industry.siemens.com/cs/ww/en/view/100777999 |
| 1/19/2016 10:59 AM | |
|
Posts: 30 Rating:
|
Ahaaa That sounds great, will try it later. Many thanks for all the answers :) |
| 1/20/2016 10:39 AM | |
|
Posts: 30 Rating:
|
Installed Sp3 yesterday and now it works fine, once again thanks for all the help. |
This contribution was helpful to
|
|
Follow us on