(1)| 2/11/2016 2:11 PM | |
|
Joined: 12/18/2014 Last visit: 1/18/2026 Posts: 36470 Rating:
|
Here is a simple example of using the PI controller. The input I1 is switched between manual and automatic mode of the controller. The setpoint can be changed via the display. AttachmentPI-controller.zip (423 Downloads) |
This contribution was helpful to
|
|
| 2/11/2016 2:47 PM | |
|
Posts: 17 Rating:
|
Thank you ixo. I'll take a look but it will certainly help. |
| 2/11/2016 6:32 PM | |
|
Joined: 12/18/2014 Last visit: 1/18/2026 Posts: 36470 Rating:
|
A small example of the power on / off with a hysteresis range. The threshold values can be set via the display.
AttachmentON_OFF.zip (386 Downloads) |
| 2/12/2016 10:26 AM | |
|
Posts: 17 Rating:
|
But first i just want to replace the sensor and make an on/off system to see if it works. Tank you |
| 2/24/2016 8:48 AM | |
|
Posts: 4757 Rating:
|
New question published by Le Test !! is split to a separate thread with the subject Best Ultrasonic sensor for a tank of water. Best regards |
| 2/24/2016 1:50 PM | |
|
Posts: 120 Rating:
|
here you are program for example
AttachmentCircuit Diagram1.zip (401 Downloads) |
Follow us on