(0)| 2/17/2016 10:51 AM | |
|
Posts: 3 Rating:
|
hi everyone.. Actually i wanted to configure an Ethernet module
(CP243-1) in S7 200 (CPU224XP CN), i uploaded the program from CPU and
Configured CP module through Ethernet wizard but i do have the same
problem while downloading. See the below attachment. (There are wizard configurations that do not match the attached modules. Reposition intelligent modules or exit and reconfigure using the wizard) I added the CP243-1 and the position is 4, and iam configuring a Server connection, and number of connections are 2 , then what should i give in TSAP (remote properties(client). Thank you in advance..
------------------------------------------------------------------------------------------ AttachmentNew Microsoft Office Word Document.docx (710 Downloads) |
Last edited by: vsubbu at: 2/17/2016 10:55:52 AMLast edited by: vsubbu at: 2/17/2016 10:57:55 AMLast edited by: Min_Moderator at: 2/18/2016 3:43:34 PMNew subject after splitting |
|
Follow us on