2/26/2016 11:35 AM | |
Posts: 15 Rating:
|
Hello I am using both SIMOCODE DP/PRO V in our plant.I am able to communicate with all of them via CP5512 (Profibus) interface from one point whether they are running or not running. Now my problem is that I am not able to change any parameter (overload,and other settings) via the CP5512 (Profibus) interface , I just get an error even if the SIMOCODE is not running. Is there any setting I need to look at on the PG/PC interface ? See attached ------------------------------------------------------------------------------------------ AttachmentDoc9.doc (308 Downloads) |
Last edited by: Min_Moderator at: 2/26/2016 1:07:13 PMNew subject after splitting |
|
2/29/2016 12:05 PM | |
Joined: 5/17/2010 Last visit: 8/20/2025 Posts: 226 Rating:
|
Hello, Please have a look at the following FAQ (it is for SIMOCODE pro but it is similar to SIMOCODE-DP) https://support.industry.siemens.com/cs/de/en/view/95157975 There is one difference for SIMOCODE-DP: Best Regards |
------------------------------------------------------------------------------------------------ |
|
Follow us on