(1)| 4/18/2016 9:05 AM | |
|
Posts: 69 Rating:
|
Hi, I am having the same problem with Siemens HMI. I am not able to download and the download stops with error. Now when I am rebooting the HMI its only showing the blank screen and not showing TRANSFER, START & CONTROL PANEL. Could you please let me know how to resolve this. I am using KTP 400 Basic Color PN, with part no 6AV6 647-0AK11-3AX0C- D1E50303. My TIA version is V13 SP1 Update 8. Thanks, Soju ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/18/2016 2:53:37 PMNew subject after splitting |
|
| 4/18/2016 9:12 AM | |
|
Joined: 5/11/2010 Last visit: 12/17/2025 Posts: 90 Rating:
|
Hello friend, pls share the IP setting of PLC and HMI |
| 4/18/2016 9:43 AM | |
|
Joined: 4/24/2006 Last visit: 1/9/2026 Posts: 9104 Rating:
|
Hello soju, In addition, please have a look at the following link: Best regards, Wizard |
| 4/19/2016 3:52 AM | |
|
Posts: 153 Rating:
|
Hi May be some problem appear when transfer project, then the project cannot full transfer and system was error (blank) You can reset to factory setting (use prosave->OS update) then try download again |
Last edited by: KhanhLe at: 4/19/2016 3:53:06 AM |
|
| 4/19/2016 4:31 AM | |
|
Joined: 10/2/2013 Last visit: 12/10/2025 Posts: 339 Rating:
|
This type of problem normally occur when accidentally disconnect your hmi device during downloading (transfer) backup. To resolve this problem you should install your OS ofHMI with the use of prosave SW,you have to use Mac address in prosave. |
|
Technology is best when it brings people together,so we are here now :) |
|
Follow us on