4/26/2016 9:25 AM | |
Joined: 12/14/2015 Last visit: 6/10/2016 Posts: 25 Rating:
|
Hello, i have a problem . I am working with CPU 1212C DC/DC/DC , order number 6ES7 212-1AE40-0XB0. I want to safe data from one analog input for some period, example one month , in PLC memory. My idea is to read value from analog input every hour, when CPU is working and save it to some data base. Is it good idea ? Maybe i can create some array and save information in it ? Thank you! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 4/26/2016 9:59:02 AMNew subject after splitting |
|
4/26/2016 11:43 AM | |
Joined: 12/14/2015 Last visit: 6/10/2016 Posts: 25 Rating:
|
And , i need to use TimeStamp, for that input. How can i do that ? |
4/26/2016 1:54 PM | |
Joined: 12/14/2015 Last visit: 6/10/2016 Posts: 25 Rating:
|
How i can create PLC Data Type (UDT or simply structure)? |
4/26/2016 2:43 PM | |
Joined: 12/14/2015 Last visit: 6/10/2016 Posts: 25 Rating:
|
I will put in effort how much i need, because i must solve this. Thank you. |
Follow us on