(0)| 4/27/2016 10:15 AM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Hello, Perhaps the following link might help: How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS? @edit: Here you can find the cable you can use: Which connector cables are available for connecting to SIMATIC Panels? Best regards, Wizard |
Last edited by: Wizard at: 4/27/2016 10:18:00 AM |
|
| 4/27/2016 12:48 PM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello, Here's bellow a link for S7-Routing. How do you use WinCC flexible to transfer a project to an operator panel via S7 Routing? |
|
Ayman Elotaify |
|
| 4/27/2016 1:50 PM | |
|
Joined: 11/21/2007 Last visit: 1/8/2026 Posts: 2327 Rating:
|
Hello Wizard had provided you with a very useful link for identifying all types of cables that can be used with SIMATIC Panels. Pl download the Excel sheet on this page and you will get all the answers that you need. The USB PC adapter A2 provides an MPI/DP interface through the PC's USB interface. Information about the USB PC adapter A2 is available in the manual in Entry ID:68849363 The "USB PC adapter" and "USB PC adapter A2" are released only for the devices below for project downloads and operating system updates.
Cheers Navnag |
Last edited by: Navnag at: 4/27/2016 1:50:35 PMThere is no such thing as the last bug in a program |
|
Follow us on