(0)| 5/9/2016 2:41 PM | |
|
Posts: 31 Rating:
|
Hello all, <please <Help... Due to some problems I had to uninstall the starter from my pc. I uninstalled and again install the starter which I got the zip folders from siemes website. also when I checked from Help-installed devices, I can see that the ssp files related to sinamics s110 are installed. the problem that I have now is the error that starter gives to me about the accessible points in order to get the connection. I put the access point on S7ONLINE and for the set interface I put the serial cable PPI. but at the end it give the error: no devices have been found. my system is sinamics s110 with CU305 DP. and i want to conncet it to my pc by serial null cable. I know that maybe it is stupid question but it is strange that now I can not proceed the starter like before that I did!!. my starter is V4.4.1.0. Thanks in advance, Regards ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/10/2016 1:41:25 PMNew subject after splitting |
|
| 9/22/2017 9:03 AM | |
|
Joined: 1/22/2013 Last visit: 12/2/2025 Posts: 3 Rating:
|
Hi Guy! you neen install SSP_SINAMICS_V4_4_3 in vol2 of software + STARTER_V4_5_1_HF5 ( hotfix). |
Follow us on