(8)| 7/21/2016 10:00 AM | |
|
Posts: 3609 Rating:
|
Import of a technical question from the user Okod
|
| 7/21/2016 8:54 PM | |
|
Posts: 38 Rating:
|
I.e I just couldn't transfer from automatic to manual control at the commissioning box. Can anyone advice please. |
| 7/26/2016 2:17 PM | |
|
Posts: 38 Rating:
|
Thank you again and sorry for being vague as you mentioned but it was not intentionally indeed. I am trying to apply Fuzzy logic and PID controller on controlling the speed a DC motor on TIA software for academic purpose. So at an earlier level I need to be apple to read the motor velocity through PWM output when the motor is on action. Please see the attached pdf file for the kits. AttachmentMotor board 1.pdf (1108 Downloads) |
| 7/26/2016 4:50 PM | |
|
Posts: 38 Rating:
|
Thank you guys for your information and yes I recently knew that fuzzy logic on PLC for DC motor is not a worthy project, but unfortunately I have to try it. For the point of using counter as a time based, which type is it HSC or the normal counter?. On other side, in the board I have two points I0.4 & I0.5 (LEDs) that making signals when the motor cut their fields, i.e. when the motor cut any one of them 4 times that makes 1 rotation. So can I use the counter to count the speed using these to inputs I0.4 & I0.5 ? If it is possible please advice. The two LEDs are visible in the attached pic next to the rotor one of them is on and the other of. AttachmentMotor board 1.pdf (1097 Downloads) |
Last edited by: Okod at: 7/26/2016 4:54:35 PMLast edited by: Okod at: 7/26/2016 4:56:59 PM |
|
Follow us on