(0)| 7/30/2016 3:19 PM | |
|
Posts: 2 Rating:
|
Dear I am facing same problem. I have two CPU 400H in Rack 0 and 1 respectively with each one CP. I am usinf unspecified in the properties with active connection establishmnet unchecked. Before I checked the connection it was working fine but i dont know now it no longer works. Only one CP in Rack 0 is communicating not the one in Rack 1, I tried to diagnose it says 8304 error. When I connect with Modbus scan software it reads from CP-1 not from CP-2. I dont understand what is the problem. When connecting to CP in Rack 1 it gives an error connction not established. Attached is my program Please help... ------------------------------------------------------------------------------------------ Attachmentknjdski.zip (381 Downloads) |
Last edited by: Min_Moderator at: 8/1/2016 2:19:40 PMNew subject after splitting |
|
Follow us on