(0)| 9/27/2016 7:51 AM | |
|
Joined: 11/9/2008 Last visit: 1/10/2026 Posts: 414 Rating:
|
Hi All, I am using ET 200iSP interface module [6ES7 152-1AA00-0AB0] with Digital input module [6ES7 131-7RF00-0AB0]. When I am configuring DI module then DI module address occupying 3 Bytes e.g 0..2 in normal module only 1 byte is occupying. In system manual 1st byte is used for Input signal, 2nd byte used for Value status for Channel 0 to 7 and 3rd byte Unassigned. From manual I understood that 1st byte is used for Input signal but I want know about 2nd byte in details . How 2nd byte analysis whether input is valid or not valid. I didn't find any details in manual. For reference please find the attached DI module address assignment manual. Please provide some information. Waiting for reply. Regards, Yogendra AttachmentDigital input module.pdf (392 Downloads) |
| 10/20/2016 11:24 AM | |
|
Posts: 4757 Rating:
|
New question published by Msc.Automation Eng. is split to a separate thread with the subject ET-200, Error "Monitoring time for data message frame exceeded". Best regards |
Follow us on